This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CB3T3245: IBIS model shows 2.1 V on output when input is 3.3 V

Part Number: SN74CB3T3245


I hope all is well! 

 

I'm trying to simulate the SN74CB3T3245PW IBIS model but it is having some issues, please see below:

 

I seem to be running into a problem with the SN74CB3T3245PW IBIS model (your scdm055.ibs dated July 30, 2003).  When I attempt to pass a 3.3V signal through the model from pin 15 to pin 5 it comes out at only 2.1V.

 


 

Is there a newer model available? Do you have any other suggestions?

 

Thank you,

Adam

  • Hi Adam,

    The CB3T devices are designed to level shift signals - See details from the SN74CB3T3245 datasheet.

    Can you explain what you are trying to model? 

    IBIS models are for modeling logic pins and doesn’t really do a great job with signal path models.  You can use the SN74CBTLV3245A  for rail to rail switching and no level shift - It also has an IBIS and HSPice model available online.

    Let me know if you have any questions.

    Thanks

    Saminah