Hi,
I have two questions regarding TS5A3166:
1. Is there a difference between the currents of the NO and COM pins?
For instance if a 5mA current is driven from the NO pin, what is the expected current at the COM pin (and vice versa)?
2. In case of a contention, i.e. different voltages in the NO and COM pins (for instance, NO = 1.8V, COM = 5V, for several mS), how will the device react?
Thanks,
Yaron.