This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1134: Vdd=0.8V/Vss=-2.5V operation

Part Number: TMUX1134


Hi team,

My customer considers to use the device with Vdd=0.8V/Vss=-2.5 supply voltage.

And logic level is Hi=0.8V/Lo=0V.

Is this usage okay for this device?

I'm concerned about if the device and internal logic can work such a low Vdd voltage even though total supply voltage is 3.3V.

Best regards,

Shota Mago

  • Hi Shota,

    For TMUX1134, the recommended operating conditions for dual supply is Vss range to be within -2.75~ 0V, and Vdd (Single supply) to be within 1.08V~5.5V.

    So Vdd=0.8V in single supply scenario would exceed the recommended operating conditions. Please see below for the TMUX1134 datasheet recommended operating conditions

    What is your customer's application scenario?

    Thanks

    Saminah

  • Hi Saminah,

    Thanks for your reply.

    As for VDD range specified in the datasheet, it shows (single).

    Does this condition also apply to dual supply voltage?

    Best regards,

    Shota Mago

  • Hi Shota,

    This device is a 5.5V single supply or a ±2.75V dual supply mux. For dual supply, the difference between VSS and VDD need to b between 1.08V~5.5V.

    You have  total difference of 3.3V between VDD and VSS - your VIH and  VIIL specs need to be similar to the 3.3V supply Electrical Characteristics table.

    Also, to avoid any potential issues with VDD being so low, I would recommend to increase VDD to meet the min value for VDD rating of 1.08V if you are using dual supply and shift the negative rails up if you want to keep 3.3V as ±dual supply range.

     

    Thanks

    Saminah