This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1247: TMUX1247DCKR use?

Part Number: TMUX1247


I have a switch material on my side.Mainly used to select MDC, MDIO interface.Can TMUX1247DCKR be satisfied?

  • Hi Simba,

    The TMUX1247 has bandwidth of 250MHz so it should support be able to support the application with no issue. (Usually the MDIO interface clock (MDC) speed is defined for up to 2.5 MHz.)

    I would also  check the voltage requirement and configuration you need for your application to make sure they are supported by the TMUX1247 

    Regards

    Saminah