This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV4051A: versus CD74HC4051

Part Number: SN74LV4051A
Other Parts Discussed in Thread: CD74HC4051, , TMUX1208, TMUX1308

Hi,

these two devices seems interchangeable.

My customer used to use CD4051, and the signal is within 5V in some of the application, so both CD74HC4051 and SN74LV4051A are usable, should I promote which one?