Hi; Team,
This part has an injection current control.
When Sx or D of disable switch is >VDD or <GND, the injection control circuitry clamps by shunting the voltage to GND.
However, from the data sheet description, the injection current per input terminal should be limited to <50mA and the total injection current for all disable switches should be <100mA in this situation. And To meet the limitation, it is recommended to add a series limiting resister(RLIM) in datasheet, figure-15.
What is the method (calculation formula) for obtaining this RLIM resistance value?
Regards,
H.Someno