This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCIe Gen4 100MHz Clock MUX solution

Other Parts Discussed in Thread: TS3DS10224

Hi,

Looking for PCIe 100MHz clock MUX solution which can also meet PCIe gen4 clock spec.

The part should support PCI Express (2.5Gb/s), Gen 2 (5 Gb/s) and Gen 3 (8 Gb/s) clock jitter compliant,

Do you have suitable solution to suggest for? P2P with IDT 831742I is prefer, if no, any non-p2p solution can meet the requirement should be fine.

Thanks

Saminah

  • Hi Saminah,

    The best part we have to offer to compete with the IDT 831742I is the TS3DS10224. 

    This part can be used as a high speed (Up to 720 Mbps)  4:1 Mux that then leads into a fan-out buffer, which the TS3DS10224 can be used again as a 1:2 fanout buffer. 

    See the datasheet for the part here

    Best Regards,

    Parker Dodson