Part Number: TMUX1574
while answer please consider also the case JTAG is not connected and signals need external PU/PD.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMUX1574
while answer please consider also the case JTAG is not connected and signals need external PU/PD.
Erez,
When the JTAG driver is not connected, external pull-up and pull-down resistors will be needed but only on one side of the mux: either S1-4A/B, or on the output D1-D4. The integrated pull-down resistors are only built into the control logic pins, not the signal path, and since the JTAG driver is disconnected, pull-ups will be needed on the signal path because the push-pull architecture of the driver is not present.
Hope this helps,
Regards,
Tyler