Other Parts Discussed in Thread: TMUX1511
We use SN74AHC4066 ( QFN − RGY) in our product to switch signals between camera and lens. Power supply from camera is 5V, signal levels are normally in 0 - 5V range.
The problem is that appx. 1 in 30 our products fails with end users (while successfully tested on several cameras before sending) and according to our tests it's SN74AHC4066 which starts to behave strange.
We suspect that it happens when camera is turned off and signal levels becomes appx 1V higher than power supply. (VCC = 0, signal = 1V). But we are not able to reproduce this situation in controlled environment, it happens randomly with camera and lens only. It means, if we apply 1V to signal line with Vcc = 0, it does not break the switch.
Usually our product stops working, then after a day or two it is back to normal. In rare cases we can "break" our product by removing battery from camera, and then "fix" the product by turning it on and off several times.
Another example: normally voltage drop (measured with multimiter in diod mode) between signal line and 0 is 1.6V. But "broken" switch has only 0.1V. When we heated the switch to 100 C, the voltage drop returns to 1.6V and our product starts to work correctly.
We also once registered 0.02V voltage drop between signal lines.
The strange thing is that most our products "fix" themselves while traveling back from our customers to us.
That is very frustrating and your help would be very much appreciated.