Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3L301: Can I use TS3L301 for LVDS 2:1 switch?

Part Number: TS3L301

Hi, sir

currently, I want to find a MUX switch for 8lans LVDS signal, 2 groups in, 1 output. 

can TS3L301 do it?

Br

zhangtao

  • Hi Zhang,

    To clarify the system requirements are you talking about having 8 input lanes and 4 output lanes?

    If I am understanding that the application correct, then this part should work fine for the application. LVDS is driven by a constant current, so I don't think you have to worry about voltage loss over the switch, the bandwidth for the switch is 900MHz which should be sufficient for LVDS. 

    If I am misunderstanding the application please let me know!

    Best,

    Parker Dodson