PLEASE PROVIDE TE PULL UP OR DOWN VALUE OF RESISTOR REQUIRED FOR SELECT LINE..
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The input leakage current is at most 1 µA, so to keep the voltage drop from that current below 0.5 V, the resistor must be smaller than 500 kΩ.
The TS3L301 itself has no other requirements. You can choose the value while balancing power usage and noise sensitivity, or just use 10 kΩ.
Harsh,
As Clemens said, there isn't an exact value that you need but rather a range. The aim is to mitigate the current while also keeping the voltage drop minimal.
There's some good documentation here:
https://www.ti.com/lit/an/slva485/slva485.pdf?ts=1598452469010
Thanks,
Rami