Other Parts Discussed in Thread: TMUX1204, TMUX1104
To whom may it concern.
Hi I'm HS.
I have four 1pps as inputs and need to select one signal as needed.
So i thought 4 to 1 mux would be great.
But the on time of these 1pps signals is usually short as 10ms ~ 100ms.
I found out that most mux have ac characteristics regarding duty, such as 40%~60%(typ. 50%).
Since 1pps signal can't meet that requirement, i was considering analog/digital switches. But I'm not sure which one would be ideal.
I want you to recommend mux or analog/digital switches for 4 1pps inputs.
I would really appreciate if you explain difference between analog and digital digital switches briefly and tell me which one would be better for 1pps timing solutions.
Thank you