This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1237: About IBIS model loading error

Part Number: TMUX1237


Hi.

I want to use the IBIS model of TMUX1237 on the simulator.
The simulator used is ADS(Keysight).
However, when the IBIS model is read, the following error message appears and it cannot be used.
-------------------------------------------------- -------------------------------------------------- -------------------------------------
The model'gnd' in file'D:\USER\model\TMUX1237_ibis_scdm235a\tmux1237.ibs' has the following data errors.
Simulation errors will occur if left unchanged.
Please select a different pin-model combination.

ERROR-Model'gnd' not found in the IBIS file'D:\USER\model\TMUX1237_ibis_scdm235a\tmux1237.ibs'
-------------------------------------------------- -------------------------------------------------- -----------------------------------------
When the pin information of the read IBIS model is confirmed, the same error message as below appears for S2, S1, and D.
Also, S2, S1, D were displayed as NC pins.

-------------------------------------------------- -------------------------------------------------- -----------------------------------------
The model'nc' in file'D:\USER\model\TMUX1237_ibis_scdm235a\tmux1237.ibs' has the following data errors.
Simulation errors will occur if left unchanged.
Please select a different pin-model combination.

ERROR-Model'nc' not found in the IBIS file'D:\USER\model\TMUX1237_ibis_scdm235a\tmux1237.ibs'
-------------------------------------------------- -------------------------------------------------- -----------------------------------------
It seems like there is a data error in model. How can I resolve this issue?

  • Hi,

    The IBIS model included only includes models for buffered inputs of the device. For the TMUX1237, the only buffered inputs are the select pins, which are modeled in this IBIS model, no other pin is modeled in the IBIS model. 

    Best,

    Parker Dodson