This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3A27518E: Does the TS3A27518E support SDIO Spec 50MB/s (SDR50, DDR50)?

Part Number: TS3A27518E
Other Parts Discussed in Thread: TXS02612

E2E,

Does the TS3A27518E support below data rate?

SDIO Spec

50MB/s (SDR50, DDR50)

 

My customer said they saw the TXS02612 but the part is too old.

Do you have suggestions?

Thank you,

Adam

  • Hi Adam,

    The TS3A27518E supports a typical bandwidth of 240MHz, which can support either the 50 MHz Clock for DDR50 and the 100MHz for SDR50. 

    This part was designed to help facilitate switching for qSPI and SDIO, so this is good choice for the application.

    Best,

    Parker Dodson