I do not see it is written in datasheet, even the figure shows. Can someone confirm with me whether this SN74CBTLV3251 is bi-directional?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I do not see it is written in datasheet, even the figure shows. Can someone confirm with me whether this SN74CBTLV3251 is bi-directional?
All analog and FET switches are bidirectional. (A closed switch behaves the same as a small resistor.) See Switches and muxes: Are switches & multiplexers bidirectional?
Daniel,
Clemens is on the mark with this one. The SN74CBTLV3251 is a FET switch so the signal can pass through from either direction just the same. All the source and drain pins also offer the powered-off protection (Ioff), so you can run this device in either direction you need with the same features supported both ways.
Rami