This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3L110: Recommend 1G-Ethernet switch

Part Number: TS3L110
Other Parts Discussed in Thread: TMUX1574

Hi,

My customer wants to use 2 TS3L110 as 1GHz Ethernet switch.  Can he use TS3L110s and work well? 

Also, if you have any other alternative solution, please advise us.

Thanks and best regards,
M.HATTORI.

  • Hello,

    Thank you for your question. TS3L110 has 500 MHz bandwidth and therefore does not support 1GHz Ethernet. 

    For a high-speed 4-channel 2:1 switch, I recommend using TMUX1574. TMUX1574 is an excellent device for this application because it supports up to 2 GHz signals and includes features such as powered-off protection and 1.8V logic compatibility.

    Please let me know if you have any additional questions about TMUX1574!

    Regards,
    Kate