This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV3126: FET bus switch Output enable Logic low or High

Part Number: SN74CBTLV3126
Other Parts Discussed in Thread: SN74CBTLV3125,

Hi,

We are planning to use your FET bus switch SN74CBTLV3126PWR and we have checked the Table 1. Truth Table and it is mentioned High is enable and Low is disable.

Whereas in the overview (Page 08) it is mentioned " The FET multiplexers and demultiplexers are disabled when the output-enable (OE) input is high". These both are contradictory.

Please confirm to enable the switch what is OE pin state? We need to A and B to connected when enabled.