Other Parts Discussed in Thread: TS3A44159,
Hi team,
I have a question for this part.
1. Is this part one of our devices that circumvents the excess current consumption issue mentioned here in this app note: 
It mentions that "Texas Instruments has several analog switches that are designed to accept control signals from a low-voltage microprocessor and solve the excess current consumption issue. • Analog switches with low control input threshold – These are devices with control inputs designed to have a switching threshold voltage lower than half of V+. This feature helps reduce current consumption when control signals are input from a low voltage GPIO. However, the control input threshold voltage is dependent on V+. If V+ is connected to VBATT, the threshold decreases as the battery discharges. The TS3A44159 is an analog switch that uses this type of low-voltage control inputs." Since the enable high threshold for this part is x1/3 the supply, will the excess current consumption be an issue for this part? I'm guessing not.
2. In that same document - it mentions "static current consumption". Isn't that just the leakage current when the part is OFF? So for this part it would be 50nA, is that correct?
Thanks!
Lauren