This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi sir,
what 's the value of ESD HBM & CDM for this device?
Thanks
Hello, and welcome to E2E!
Thanks for your question, please refer to the following thread:
SN74CBTLV1G125: ESD Class and Rating - Switches & multiplexers forum - Switches & multiplexers - TI E2E...
This part is an older device and does not have a specified ESD rating. However, engineering data indicates performance up to:
HBM: 1500V
CDM: 500V
I would like to recommend switching to a newer device, if possible. TMUX1101 or TMUX1102 are great options with wider supply signal range, lower Ron and leakage current, 1.8V compatible control inputs, and fail-safe logic.
If you need powered-off protection for your application, take a look at TS5A3167 which also has wider supply signal range, lower Ron and leakage current, with added powered-off protection.
Both TMUX1101 and TS5A3167 have +/-2000V ESD HBM ratings.
Let me know if you have any additional questions.
Best regards,
Kate