This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX7211: release timing

Guru 11170 points
Part Number: TMUX7211

Hello E2E,

When the release timing of TMUX7211? Our customers are looking forward it released.

Regards,
ACGUY

  • Hi ACGUY,

    I have sent you a friend request so that I can give you this information over a private message as I can't post on the public facing forum. 

    However I'd also like to point out the TMUX7212PWR is released right now - and it is the same part as the 7211 but the 7211 is active low logic while the 7212 is active high logic.

    Best,

    Parker Dodson