This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G3157-Q1: VCC/S=3.3V, A/B1/B2=1.8V, is this ok?

Part Number: SN74LVC1G3157-Q1


Dear team,

Please help to confirm the following configuration is ok?

VCC=3.3V,

S=3.3V I/O

A=1.8V INPUT I/O

B1/B2= 1.8V OUTPUT             

Or if need VCC and S are both 1.8V ?

Thanks & Best Regards,

Sherry