Other Parts Discussed in Thread: TS3A27518E
e2e,
I'm looking for a 5bit I2S selector(MCLK, LRCLK, BCLK, DIN and DOUT). Originally the request was 4bit, I used SN3257-Q1, but now need 5bits.
Below is the requirements. Could you suggest the best solution?
- Clock frequency is less than 50MHz
- Need EN function.(floating output)
- As small as possible.(2pcs of SN3257-Q1 is one of candidate because mixing two device makes latency gap)
Thank you,
Adam