Other Parts Discussed in Thread: LSF0108
Hi There,
We are considering the adoption of "SN74TVC3010".
I want to check how to use it.
[conditions]
・Each FPGA operates voltage at 1.8V.
・FPGA (A) and either FPGA (B) / FPGA (C) communicate.
・The communication speed is 33MHz.
・Communicate in both directions.
【Check】
1.Is it possible to level translation of 33MHz ?
2.Is a circuit configuration that connects in parallel acceptable ?
3.Is data communication (33MHz) possible with the configuration of the attached document?
Best regards
- satoshi