This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV3257: Bus switch

Part Number: SN74CBTLV3257
Other Parts Discussed in Thread: TS3A24157, TMUX1574, , TS3A5223, SN3257-Q1

Hi team,

My customer is looking for a Bus switch. 

  • Requirement

-Switch type : SPDT

-Number of channels : 4bit or 2bit*2

-Power supply : 3.3V for both input and output (not required tolerant)

-Signal frequency : 20MHz

-Low cost

-Small package

The customer found SN74CBTLV3257PW(4ch) and TS3A24157(2ch) series. If you have other recommended devices which are lower cost and smaller package, could you let me know?

Regards,

Yamaguchi

  • The TMUX1574 has the same price and size as the SN74CBTLV3257, but has better characteristics.

    The TS3A5223 is cheaper and smaller than the TS3A24157. (But a single 4-channel device is even cheaper and smaller.)

  • Hi Yamaguchi-san,

    The TMUX1574 is the newest 4ch 2:1 (SPDT) switch that has wider operating voltage (1.5V to 5.5V), wider operating temperature (-40C to 125C) and additional features like 1.8V logic compatibility, Fail-safe logic etc.

    The device is available in three package options: small leaded SOT-23 package (TMUX1574DYYR), UQFN package (TMUX1574RSVR) and leaded TSSOP (TMUX1574PWR) and is P2P compatible to the old SN74CBTLV3257.

    Additionally, there is a new automotive qualified variant available based on application need (SN3257-Q1).

    Hope this helps.

    Thank you,


    Regards,
    Sandesh