Hi there,
I am interested to find out if the component can be used in Class 2 medical devices.
Also if it is possible, the operating relative humidity (RH) and operating pressure.
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
I am interested to find out if the component can be used in Class 2 medical devices.
Also if it is possible, the operating relative humidity (RH) and operating pressure.
Thank you!
Hi Michelle,
The device is available in catalog/automotive/Enhanced product category but has not gone through any special certification process.
We do not specify the operating RH for devices but we do provide the qualification information and conditions used - HAST (highly accelerated stress test) in this case. During these tests the product is subjected to stringent Humidity/Pressure/Temperature per JEDEC specification and AEC-Q100 specification for automotive qualified devices. The stress conditions are listed in the qualification summary.
You should be able to pull the qualification summary at link below using the complete orderable part number.
https://www.ti.com/qualificationsummary/qualsumm/home?actionId=2800
We have a automotive qualified device - TS5A3159-Q1 and Enhanced product TS5A3159-EP that go through controlled Fab and Assembly process.
Hope this helps.
Thank you,
Regards,
Sandesh