This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1574: Default condition of pin 9 and pin 12

Part Number: TMUX1574


Hi team,

Is the default condition of pin 9 and pin 12, which refer to D3 and D4, high impedance when these pins are not connected?

Best regards,

Wendy

  • HI Wendy,

    The Dx pins are Hi-Z only when EN/ = 1 (H) i.e. chip is not enabled (Table 1, truth table in datasheet). During this time the channel SEL pin has no influence on the switch status.

    If EN/ = 0 (L), depending on the SEL pin condition either Dx to SxA channels or Dx to SxB channels will be connected. Under this condition the Dx pins will not be Hi-Z but the non-connected Sx channel will be Hi-Z depending upon the switch status.

    Ex: if the Dx is connected to SxA, EN/=- (L) + SEL = 0 (L), the SxB side switch will be OFF and vice versa.

    Hope this helps. Let me know if any further questions.

    Thank you,


    Regards,
    Sandesh

  • Hi Sandesh,

    Thank you so much for your help!

    Best regards,

    Wendy