This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5MP646: (TMUX646 Pin-to-pin upgrade supporting 6-GHz bandwidth available) ts5mp646 for 2 input and 2 output

Part Number: TMUX646TS5MP646
Other Parts Discussed in Thread: TS5MP646

Hi team,

my customer wants to achieve below 2 options with ts5mp646.

Case 1, A<---> B,  C<---> D

Case 2, A<---> D,  C<---> B

Can below solution work?

  • HI Hollis,

    The above solution will work functionally.

    Please note that the R & C will be doubled on each channel as there are two back to back / series connected devices and need to take that into account while designing the system. Mainly switch RON will be doubled, some impact on timing and bandwidth due to RC component and the PCB layout itself.

    Overall, this is an acceptable use case.

    Thank you,


    Regards,

    Sandesh