My customer is using the TS12A4516 (DBV) in a design. I attached an image showing the implementation (internal link)
They are going to production now, but have been seeing a 2~3 issues a month - and finally think they found the cause.
They do a final operation check before shipping - and during these tests, they see a fault.
The fault seems to happen because the TS12A4516 does not properly connect the output COM to NC, and the processor looking at the NC detects the open-state. The High-Voltage supply should be turned on, and supplying power to the load, but because the switch isn't connecting COM to NC, this isn't detected.
Take a look at the image, and let me know if there are any concerns with the setup, or something specific to the device that needs to be taken into consideration.
Thanks,
Darren