This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX6219-Q1: Can the TMUX6219-Q1 device handle pulses of 300mA for 1.5µs followed by 1mA for 30µs @ 15V DC

Part Number: TMUX6219-Q1


e2e, 

  1. Can the TMUX6219-Q1 device handle pulses of 300mA for 1.5µs followed by 1mA for 30µs @ 15V DC? I assume, the only limitation is the thermal performance/power losses, right?
  2. Do you have curves showing the max R_DSon in dependence of Vsup (12V – 23V is of interest)? Or can I do a linear interpolation between the data points of 12V / 32V given in the data sheet?
  3. Do you have a Spice model?

Thank you,

Adam