Hello I would like to use this part number in order to switch a differential clock PCI-e GEN 5 while the device will be RC or EP
will it work ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello I would like to use this part number in order to switch a differential clock PCI-e GEN 5 while the device will be RC or EP
will it work ?
Hi Itzik,
From a bandwidth perspective this will work for this device as it supports up to 300MHz, however, what is the voltage of the signal you are passing? This device supports up to 3.3V. Also, do you need a 4 channel, 2:1 switch (like the one you suggested, TS3A5018)? Or do you just need a single channel, 2:1 switch?
Thanks!
Bryan
I would like to mux PCI-e Gen 5 clock which is a differential clock and the voltage is 0 - 0.7V
Hi Itzik,
In that case, the TS3A5018 will be fine for this application. Let me know if you have any other questions!
Thanks!
Bryan