This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX6219: Negative Common Mode for CAN termination resistors

Part Number: TMUX6219

Do you know if it is possible to switch CAN termination resistors with our switches?

This would be to adjust the termination, the common mode range is +-12V

Could this or another recommended device could handle/switch at negative common mode?

Thanks,
Jon

  • Hi Jon,

    Could you help with the questions below so that we understand the requirement.

    - Is this for Industrial or Automotive application?

    - Do you know the CAN transceiver device that the customer is using in their system? 

    - What voltage rails are available in the system?

    Thank you,


    Regards,
    Sandesh