Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC4066: SN74HC4066 multiplexing I2C signal to solve EEPROM I2C address conflict

Guru 16770 points
Part Number: SN74HC4066
Other Parts Discussed in Thread: TS3A24157, TCA9543A

Hi

Let me consider SN74HC4066 as use for I2C signal switching as follows.

What is the issue that would be supposed?

I believe we can offer the better solution if we use TS3A24157 as alternative.

However, we want to confirm whether the upper figure using SN74HC4066 has problems or not.

Could you tell me your view?

BestRegards

  • Na Na,

    What are you trying to accomplish with this circuit?  The I2C bus has the ability to place multiple slave devices on the same I2C bus.  The I2C protocol has an address byte to select which slave device to select between so I don't know why you would need an 1:1 SPST switch like the SN74HC406  

    Here is a good app note Understanding the I2C bus I found in the I2C e2e forum that explains I2C addressing in more detail.

    If your slave devices have the same I2C address and you are trying to isolate them for proper communication I would recommend looking at this appnote that talks about how to solve this issue with devices like the TCA9543A.  

    How to select the correct I2C device

    Thank you,

    Adam

  • Hi Adam

    Thank you for your reply.

    ROM is EEPROM for configuration of Timing Controller (master).
    These two EEPROMs can't be set different address, so placing them on the same I2C bus wouldn't be supported by the master device.

    We are trying to isolate SCL1/SDA1 and SCL2/SDA2 channels using SN74HC4066 device like the figure.

    I think this configuration might not be reasonable way, but this is the most inexpensive way that we could take.

    So if possible, could you please indicate issues and tell us why this configuration is not practical?

    BestRegards
  • Na Na,

    I do not see an issue with the schematic you have above. If the SN74HC4066 device is the lowest cost solution for you it will isolate the I2C bus since the two EEPROMs can't be set different address.

    Adam