This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello support team,
Our customers is evaluating TS3A5223 now.
In the customer's circuit as shown in the figure, 1.8 V is supplied to Vcc, and the voltage generated from 3.3 V is applied to COM1 at Vcc = 1.8 V.
When SEL1 is 'H', voltage at NO1 is as expected at 1.65V.
When SEL 1 is 'L', voltage at NO1 should be 0 V, but it is around 1.15 V.
It seems that the switch does not turn off and leaks.
In the data sheet, the upper limit voltage of the input terminals NOx and COMx is not limited by Vcc.
However, I think that these input voltages have no tolerance above Vcc.
Is my understanding wrong?
Best regards,
M. Tachibana
Tachibana,
You have found a datasheet error in the TS3A5223 device. Devices it this family to have protection diodes from COM to Vcc. If you are operating Vcc at 1.8 V and supplying the COM pin with 3.3 V we would expect to turn on the protection diode and that would be where you are leaking your current from COM to Vcc. I will order some of these parts so that I may test them to confirm our suspicions and correct the datasheet.
What are you trying to do in your application with the switch? Maybe we can help you find an alternative device like a voltage level shifter?
Thank you,
Adam
Tachibana-san,
No, you have come across a datasheet error. The recommended operating conditions should look similar to the TS3A24159 which states the recommended operating voltage is limited by the supply voltage. The reason is there will be protection didoes that will begin to conduct if the signal on the pins is greater than the supply voltage. We are still tying to make this change in the datasheet but it will take some time.
Thank you,
Adam