Other Parts Discussed in Thread: AFE4490, AFE4400, TS3DS10224
Hi. I want to use switch ic or mux to select photodiodes.
The ten photodiode are used.
Photodiodes is photovoltaic mode, TIA is AFE4400 or AFE4490.
switch frequency is 1000Hz or 2000Hz.
Only one photodiode is selected and the others are not selected.
The photodiode is ODD-5WB opto diode.
1) would you recommend me to adequate switch or mux?
2) Is there any problem?