Other Parts Discussed in Thread: TMS320C6747
Hi, I'm trying to connect to TMS320C6747 on a custom board. I'm using JTAG to USB converter, XDS510 PLUS. I got the following error:
Error connecting to the target:
Error 0x80000244/-2131
Fatal Error during: Register, Initialization, OCS,
Cannot access register at 0x00000000
I/O Port = 510
Board Name: EVMC6747_XDS510USB
Cpu Name: IcePick
Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.
Correct me if I'm wrong but I believe I do not need GEL file to connect. What am I missing here? Please help.
Regards,
taiyc