Part Number: TM4C1297NCZAD
Tool/software: Code Composer Studio
I almost have my development environment set up with Code Composer 6.2.0.00050 and the TM4C129X Development Board connected to our controller board. I am able to build the code and download it to the target without any problems (as far as I am aware). I can also start running the code, but then I get these messages.
CORTEX_M4_0: Error: Debug Port error occurred
CORTEX_M4_0: Trouble Halting Target CPU
Any ideas where to look?