Other Parts Discussed in Thread: CC3200, CC3200SDK, CCSTUDIO
Hi All,
I am experiencing random code halts running on CC3200 Launchpad.
I have the Launchpad connected via USB (no external debugger).
Running the code using CCS 6.1.2 (Win 7).
When the code halts I see "Cortex_M4_0: Error: Debug port error occurred." in the CCS console.
The code loads fine, code halt/error happens during execution, sometimes within 10 minutes, sometimes within 10 seconds.
It's not related to which code I am executing. (random halts/error with any of the TI demos I tried, or My "Hello world" to console in a loop).
Reading some of the posts, I stepped back to running unmodified TI blinky demo. (Results: Same random code halts and error)
Sometimes I can continue the code with F8, most of the time I just get more errors and halts which are not recoverable..
Code is halting in different locations of "No source available for 0x....".
Looking at disassembly, sometimes I see a location and function names that can be reasonably traced back to main.c of blinky
I have tried 2 different desktop PC's, 2 different CC3200 launchpads, 2 different USB cables (ones supplied by TI with the board).
I'm not connected to USB hubs, but direct to PC USB.
The CC3200.xml file is from the SDK (C:\TI\CC3200SDK_1.1.0\cc3200-sdk\tools\ccs_patch)
SOP (J15-J17) jumper are open
J8-J11 Shorted
J6-J7 Shorted 2-3
D2 LED stays on
I assume there is something I am missing, but I am not seeing things to try that I have not tried.
Any help would be appreciated.
Thanks.