Part Number: TMS320C6745
Tool/software: Code Composer Studio
Hello,
I'm trying to debug a custom board using the TMS320C6745 using the TI-XDS100V2 programmer and keep getting the following error:
C674X_0: Error connecting to the target: (Error -6311) PRSC module failed to write to a register. (Emulation package 7.0.188.0)
When I run the "Test Connection" function, no problems are identified. I have searched other threads regarding this error and see that this error most likely has to do with a hardware issue, but cannot seem to identify any faults in my design.
I am using CCSv8 and have my JTAG interface connected as shown below. Not sure if it's relevant or not, but my boot pins are configured for booting from SPI0 Flash using pull up/down resistors.
Any suggestions on how to approach this?
Thanks,
Matt