Part Number: TIDA-01604
Other Parts Discussed in Thread: C2000WARE, POWERSUITE, CCSTUDIO
Tool/software: Code Composer Studio
Hello,
I am having difficulties in getting the CCS solution adapter to fully start to be able to customize a design using the TIDA-01604 reference design as a start. I installed the C2000Ware_DigitalPower_SDK.
When I open the solution adapter, I get to to the "Select Options" portion, but am unable to get further to the "customize solution' portion. When I click on the design (6.6kW CCM PFC TTPL 1PH: F28004x) nothing happens, and no errors are thrown.
I followed all of the steps in the troubleshooting FAQ:
- Ensured GUI composer run-time is installed.
- Ensured powerSUITE is installed
- Made sure there is no space in the file path: (C:/ti/c2000/powerSUITE_2_05_01_00)
- Made sure .NET is up to date
- Running English (United States) Language pack in Windows
See included screenshot for some more settings.
Anyone have any ideas? This is running CCS 7.4.0.00015