Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] CCS: Stack Usage view in CCS 9.3.0 under Linux displayed incorrectly unless apply work-around for EXT_EP-9563 of setting SWT_GTK3=0

Tool/software: Code Composer Studio

With CCS 9.3.0 under Ubuntu 18.04.4 LTS the Stack Usage view wasn't displaying the Inclusive Size column. E.g.:

If set SWT_GTK3=0 prior to starting CCS, which is the work-around for CCS IDE flickers on mouse movement when ROV and ReX is opened on Linux, then the Inclusive Size is displayed:

Is it worth updating the description of EXT_EP-9563 or the [FAQ] Certain views like the Getting Started view, App Center, Resource Explorer, and Code Analysis views are blank in CCS Linux. How do I fix this? to mention that the Stack Usage view is also affected?

  • Hello Chester,

    Thanks for reporting this issue. Despite the same root cause, I filed a separate issue for this since the symptoms are different.

    the Tracking ID is: EXT_EP-9739

    I also FAQ'ed this thread.

    Thanks

    ki