Part Number: TIDA-00961
Tool/software: Code Composer Studio
Hello, recently I have been studying the TIDA-00961 [High-Efficiency, 1.6-kW, High-Density, GaN-Based, 1-MHz CrM Totem-Pole PFC Converter Reference] and met many questions.
Firstly, I will tell the change that I hava made based on the Reference CCS project. All changes are in File SETTING.H. Since I donn't need too high frequency, so I lower the MIN_PFC_PWM_SWITCHING_FREQUENCY to 20*1000 and MAX_PFC_PWM_SWITCHING_FREQUENCY to 200*1000. However, something seems to be wrong that the PWM cannot refresh. So I changed PFC_PWM_PERIOD to 19*1000, then the switching frequency seems to be right.
Fig 01. 02. the constant frequency while the TBPRD is refreshing
Secondly, I have verified the feasibility in DC/DC condition with current and voltage loop closed. However, when I change it to AC/DC with closed current loop, the PWM is wrong again which is shown as below.
Finally, since the author of the CCS project is Hrishi Nene, I will very appreciate it if he/she can anwser my questions. Of course, if my CCS project and schematic are needed please tell me, I can send them to you.
Fig 03. the wrong PWM (high frequency)
The problem confused me for a long time and the project is very very important to me.
Thank you very very much.