I am trying to install the code composer studio from the cd that gave me the lecturer I get error saying "Error1327 invalid drive C:\" I think that the problem is because I didn't install windows on drive C it is on different drive, I tried to change the destination of the folder the problem is that when I click on Code Composer Studio v3.1.
-follow the steps to the screen that is labeled 'Select Installation Type' and click 'Custom Install'.
-This will allow you to browse and select the destination folder for your installation.
what can I do? is there a way to change the drive letter manually? is there a way to remove th error I get so it would permit me change the destination of the windows folder?