Other Parts Discussed in Thread: MSP430F169
Hello,
I am currently working on an MSP430F169 and CCS V5. I have this error when I want to run my project :
error #10269: output file "project .out" exceeds code size limit
error #10010: errors encountered during linking; "project .out" not
So I check the .map file and I have 15KB of free space left:
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
SFR 00000000 00000010 00000000 00000010 RWIX
PERIPHERALS_8BIT 00000010 000000f0 00000000 000000f0 RWIX
PERIPHERALS_16BIT 00000100 00000100 00000000 00000100 RWIX
RAM 00000200 00000800 000000de 00000722 RWIX
INFOB 00001000 00000080 00000000 00000080 RWIX
INFOA 00001080 00000080 00000000 00000080 RWIX
FLASH 00001100 0000eee0 0000b200 00003ce0 RWIX
INT00 0000ffe0 00000002 00000000 00000002 RWIX
INT01 0000ffe2 00000002 00000000 00000002 RWIX
INT02 0000ffe4 00000002 00000000 00000002 RWIX
INT03 0000ffe6 00000002 00000000 00000002 RWIX
INT04 0000ffe8 00000002 00000002 00000000 RWIX
INT05 0000ffea 00000002 00000002 00000000 RWIX
INT06 0000ffec 00000002 00000002 00000000 RWIX
INT07 0000ffee 00000002 00000002 00000000 RWIX
INT08 0000fff0 00000002 00000000 00000002 RWIX
INT09 0000fff2 00000002 00000000 00000002 RWIX
INT10 0000fff4 00000002 00000000 00000002 RWIX
INT11 0000fff6 00000002 00000000 00000002 RWIX
INT12 0000fff8 00000002 00000000 00000002 RWIX
INT13 0000fffa 00000002 00000000 00000002 RWIX
INT14 0000fffc 00000002 00000000 00000002 RWIX
RESET 0000fffe 00000002 00000002 00000000 RWIX
Then I check the CCS licence and I have a full one :
So I don t understand this error. I don't know if it comes form CCS or the MSP430 ?
Should I improve or update my licence ?
I try to Activate CCS :
but the procedure ask me Activation ID, and I do not have that.
So is it a licence problem ? and if yes how can get an unlimited licence ?
should I buy this
Regards