Hi Team,
my customer has an error with flexlm license server on Win 7. The error message is "(lmgrd) tidspssw exited with status 123 ()". You can find the message in the log file in the appendix:
12:29:29 (lmgrd) ----------------------------------------------- 12:29:29 (lmgrd) Please Note: 12:29:29 (lmgrd) 12:29:29 (lmgrd) This log is intended for debug purposes only. 12:29:29 (lmgrd) In order to capture accurate license 12:29:29 (lmgrd) usage data into an organized repository, 12:29:29 (lmgrd) please enable report logging. Use Flexera Software LLC.'s 12:29:29 (lmgrd) software license administration solution, 12:29:29 (lmgrd) FLEXnet Manager, to readily gain visibility 12:29:29 (lmgrd) into license usage data and to create 12:29:29 (lmgrd) insightful reports on critical information like 12:29:29 (lmgrd) license availability and usage. FLEXnet Manager 12:29:29 (lmgrd) can be fully automated to run these reports on 12:29:29 (lmgrd) schedule and can be used to track license 12:29:29 (lmgrd) servers and usage across a heterogeneous 12:29:29 (lmgrd) network of servers including Windows NT, Linux 12:29:29 (lmgrd) and UNIX. Contact Flexera Software LLC. at 12:29:29 (lmgrd) www.flexerasoftware.com for more details on how to 12:29:29 (lmgrd) obtain an evaluation copy of FLEXnet Manager 12:29:29 (lmgrd) for your enterprise. 12:29:29 (lmgrd) 12:29:29 (lmgrd) ----------------------------------------------- 12:29:29 (lmgrd) 12:29:29 (lmgrd) 12:29:29 (lmgrd) pid 580 12:29:29 (lmgrd) Done rereading 12:29:29 (lmgrd) FLEXnet Licensing (v11.10.1.0 build 99220 x64_n6) started on DEFTHW99Y11SRV (IBM PC) (5/14/2014) 12:29:29 (lmgrd) Copyright (c) 1988-2012 Flexera Software LLC. All Rights Reserved. 12:29:29 (lmgrd) US Patents 5,390,297 and 5,671,412. 12:29:29 (lmgrd) World Wide Web: http://www.flexerasoftware.com 12:29:29 (lmgrd) License file(s): C:\Program Files (x86)\TI ComposerStudio\TIComposerStudio.lic 12:29:29 (lmgrd) lmgrd tcp-port 27180 12:29:29 (lmgrd) Starting vendor daemons ... 12:29:29 (lmgrd) Starting vendor daemon at port 27181 12:29:29 (lmgrd) Using vendor daemon port 27181 specified in license file 12:29:29 (lmgrd) Started tidspssw (pid 8124) 12:29:34 (lmgrd) tidspssw exited with status 123 () 12:29:34 (lmgrd) Since this is an unknown status, license server 12:29:34 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon. 12:29:34 (lmgrd) Starting vendor daemon at port 27181 12:29:34 (lmgrd) Using vendor daemon port 27181 specified in license file 12:29:34 (lmgrd) REStarted tidspssw (pid 3684) 12:29:39 (lmgrd) tidspssw exited with status 123 () 12:29:39 (lmgrd) Since this is an unknown status, license server 12:29:39 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon. 12:29:39 (lmgrd) Starting vendor daemon at port 27181 12:29:39 (lmgrd) Using vendor daemon port 27181 specified in license file 12:29:39 (lmgrd) REStarted tidspssw (pid 7432) 12:29:44 (lmgrd) tidspssw exited with status 123 () 12:29:44 (lmgrd) Since this is an unknown status, license server 12:29:44 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon. 12:29:44 (lmgrd) Starting vendor daemon at port 27181 12:29:44 (lmgrd) Using vendor daemon port 27181 specified in license file 12:29:44 (lmgrd) REStarted tidspssw (pid 1720) 12:29:49 (lmgrd) tidspssw exited with status 123 () 12:29:49 (lmgrd) Since this is an unknown status, license server 12:29:49 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon. 12:29:49 (lmgrd) EXITING DUE TO SIGNAL 1
Some additional information:
• The license server is a virtual server.
• The pathname of the license file contains spaces
The changeover to the new virtual server license was necessary because the old license server is running Windows XP and can not be switched to Windows 7. On the old Windows XP computer, the license server is running - software without problems.
Thanks and regards,
Oleg