This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with flexlm license server on Win 7

Hi Team,

my customer has an error with flexlm license server on Win 7. The error message is "(lmgrd) tidspssw exited with status 123 ()". You can find the message in the log file in the appendix:

12:29:29 (lmgrd) -----------------------------------------------
12:29:29 (lmgrd)   Please Note:
12:29:29 (lmgrd) 
12:29:29 (lmgrd)   This log is intended for debug purposes only.
12:29:29 (lmgrd)   In order to capture accurate license
12:29:29 (lmgrd)   usage data into an organized repository,
12:29:29 (lmgrd)   please enable report logging. Use Flexera Software LLC.'s
12:29:29 (lmgrd)   software license administration  solution,
12:29:29 (lmgrd)   FLEXnet Manager, to  readily gain visibility
12:29:29 (lmgrd)   into license usage data and to create
12:29:29 (lmgrd)   insightful reports on critical information like
12:29:29 (lmgrd)   license availability and usage. FLEXnet Manager
12:29:29 (lmgrd)   can be fully automated to run these reports on
12:29:29 (lmgrd)   schedule and can be used to track license
12:29:29 (lmgrd)   servers and usage across a heterogeneous
12:29:29 (lmgrd)   network of servers including Windows NT, Linux
12:29:29 (lmgrd)   and UNIX. Contact Flexera Software LLC. at
12:29:29 (lmgrd)   www.flexerasoftware.com for more details on how to
12:29:29 (lmgrd)   obtain an evaluation copy of FLEXnet Manager
12:29:29 (lmgrd)   for your enterprise.
12:29:29 (lmgrd) 
12:29:29 (lmgrd) -----------------------------------------------
12:29:29 (lmgrd) 
12:29:29 (lmgrd) 
12:29:29 (lmgrd) pid 580
12:29:29 (lmgrd) Done rereading
12:29:29 (lmgrd) FLEXnet Licensing (v11.10.1.0 build 99220 x64_n6) started on DEFTHW99Y11SRV (IBM PC) (5/14/2014)
12:29:29 (lmgrd) Copyright (c) 1988-2012 Flexera Software LLC. All Rights Reserved.
12:29:29 (lmgrd) US Patents 5,390,297 and 5,671,412.
12:29:29 (lmgrd) World Wide Web:  http://www.flexerasoftware.com
12:29:29 (lmgrd) License file(s): C:\Program Files (x86)\TI ComposerStudio\TIComposerStudio.lic
12:29:29 (lmgrd) lmgrd tcp-port 27180
12:29:29 (lmgrd) Starting vendor daemons ... 
12:29:29 (lmgrd) Starting vendor daemon at port 27181
12:29:29 (lmgrd) Using vendor daemon port 27181 specified in license file
12:29:29 (lmgrd) Started tidspssw (pid 8124)
12:29:34 (lmgrd) tidspssw exited with status 123 ()
12:29:34 (lmgrd) Since this is an unknown status, license server 
12:29:34 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
12:29:34 (lmgrd) Starting vendor daemon at port 27181
12:29:34 (lmgrd) Using vendor daemon port 27181 specified in license file
12:29:34 (lmgrd) REStarted tidspssw (pid 3684)
12:29:39 (lmgrd) tidspssw exited with status 123 ()
12:29:39 (lmgrd) Since this is an unknown status, license server 
12:29:39 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
12:29:39 (lmgrd) Starting vendor daemon at port 27181
12:29:39 (lmgrd) Using vendor daemon port 27181 specified in license file
12:29:39 (lmgrd) REStarted tidspssw (pid 7432)
12:29:44 (lmgrd) tidspssw exited with status 123 ()
12:29:44 (lmgrd) Since this is an unknown status, license server 
12:29:44 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
12:29:44 (lmgrd) Starting vendor daemon at port 27181
12:29:44 (lmgrd) Using vendor daemon port 27181 specified in license file
12:29:44 (lmgrd) REStarted tidspssw (pid 1720)
12:29:49 (lmgrd) tidspssw exited with status 123 ()
12:29:49 (lmgrd) Since this is an unknown status, license server 
12:29:49 (lmgrd) manager (lmgrd) will attempt to re-start the vendor daemon.
12:29:49 (lmgrd) EXITING DUE TO SIGNAL 1

Some additional information:
The license server is a virtual server.
• The pathname of the license file contains spaces

The changeover to the new virtual server license was necessary because the old license server is running Windows XP and can not be switched to Windows 7. On the old Windows XP computer, the license server is running - software without problems.

 

Thanks and regards,

Oleg

  • Hi Oleg,

    how did they do the migration?   Did they rehost the license?  Have they tested that it works locally and that it is seen outside the vm?   I am not sure how flexnet handles vms.

    Best Regards,

    Lisa

  • We purchased one new license and rehosted three existing licenses. License Server for the four licenses is the Virtual Server.

    We are not able to test that it works because the License daemon does not start. Here is the error message from the log - file:
    12:29:29 (lmgrd) FLEXnet Licensing (v11.10.1.0 build 99220 x64_n6) started on DEFTHW99Y11SRV (IBM PC) (5/14/2014)
    12:29:29 (lmgrd) Copyright (c) 1988-2012 Flexera Software LLC. All Rights Reserved.
    12:29:29 (lmgrd) US Patents 5,390,297 and 5,671,412.
    12:29:29 (lmgrd) World Wide Web:  http://www.flexerasoftware.com
    12:29:29 (lmgrd) License file(s): C:\Program Files (x86)\TI ComposerStudio\TIComposerStudio.lic
    12:29:29 (lmgrd) lmgrd tcp-port 27180
    12:29:29 (lmgrd) Starting vendor daemons ...
    12:29:29 (lmgrd) Starting vendor daemon at port 27181
    12:29:29 (lmgrd) Using vendor daemon port 27181 specified in license file
    12:29:29 (lmgrd) Started tidspssw (pid 8124)
    12:29:34 (lmgrd) tidspssw exited with status 123 ()

    We use this virtual server for several other flexnet licenses from other companies without any problems.

    Best regards

    Eduard Delling

  • Hi Eduard,

    what steps did you take.  Did you see this wiki and is the daemon in the correct folder?

    http://processors.wiki.ti.com/index.php/License_Server_Administration_for_CCS

    WIthout more information, some thoughts

    - is it started as a service

    - could there be an antiviru or permission issue

    - have you tried rebooting etc

    - have you verified the eth0 address and that rehosting went correctly.   


    The first step, of course is to verify it works within the VM.

    Best Regards,
    LIsa

  • Hi Lisa,

    after reinstalling the license server software as described in your document "License Server Administration for CCS" the license server is working as expected. I'm not sure what the exact reason for the error was but I'm glad that the problem is solved.

    Thanks for your support on this issue.

    Best regards
    Eduard Delling

  • Hi Eduard,

    very glad to hear.   Thanks for the update and all the best with development.

    Best Regards,
    Lisa