Part Number: TMS320F28335
Hello!
I'm Sinho, Kim.
I'm now reviewing TI's XDS100v3 Rev. 2 Design Kit for considering if for the future use.
While doing this, I have found some problems related to the kit and they are listed below.
1. After several installation of XDS100v3 Rev. 2 Design kit, XDS100v3-Rev2.exe file have not been found on the disk.
2. I couldn't have look over the FPGA design files using Libero IDE v9.1 which need a paid license.
2.1 Instead, I tried to do it using Libero SoC v11.8 with the silver license which is a free license and support all ProASIC3 devices.
2.1.1 When opening v3_fpga_2.prjx file, I have found that it looks like a blank project.
2.1.2 When opening v3_fpga_125.prjx file, I have found that it has some design information.
2.1.2.1 It was fortunate for me to see the design.
2.1.2.2 I couldn't have been sure what fpga device matches with the schematic.
2.1.2.2 When executing "Route and Place", I have found some waring messages while there was no error.
2.1.2.2.1 Because I have not studied Libero SoC v11.8 yet, I can't modify the design.
2.1.2.2.2 I think that I need the modified design file without any warning and error message.
The above statement is my problems. In summary,
1. XDS100v3-Rev2.exe file was not found on my disk after several intallation and uninstallation.
2. What fpga device matches with the schematic.
3. The project, that v3_fpga_2.prjx file includes, looks like a blank project when using Libero SoC v11.8.
4. I need the modified design, that v3_fpga_125.prjx file includes, without any warning and error message when using Libero SoC v11.8.
Could you help me about these problems?
Thank you for your attention.
Sincerely yours.
Sinho, Kim.