Other Parts Discussed in Thread: CC3220SF
Tool/software: Code Composer Studio
CCS 9.3, on Mac book pro 16"
I have only the auto-breakpoint (at main) enabled, all other breakpoints are removed. I also do not have the skip all breakpoints option set. When I click the debug button, project compiles and gets downloaded to the target but then nothing happens or sometimes I get: "AutoRun: Target not run as breakpoint could not be set: Exception error from JobMgr member function call". Then when I press the debug button again, it requester comes up with "you are required to terminate ... etc", I press No. And now CCS appears to set at main() and the step into, step over etc. debug buttons are available. I can step through just fine.
Resetting/restarting CCS and/or computer makes no difference. USB connector/cable appears fine to me. There is nothing else connected to the board.
This behavior just started as of this morning and is rather frustrating - to say the least.