This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TM4C1294KCPDT: XDC_CG_ROOT Path Variable - how it is decided which xdc tool path to be used if there are multiple xdc tools are installed on the system.

Part Number: TM4C1294KCPDT


Tool/software: Code Composer Studio

Dear SupportTeam,

In our Project Properties, previously it showed "C:\ti\ccs901\xdctools_3_55_00_11_core" but it automatically changed to "C:\ti\xdctools_3_32_00_06_core" after executing "Rediscover" option. Why did this happen?

Thanks & Regards

Abhijit