This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems in running a program without CCS from flash

I have designed a code using CCS v 3.3 compiler. I am using F28335 controller and Black Hawk emulator. whenever I burn the program using On-chip flash programmer and press run, the program runs absolutely fine but when I detached the emulator (i.e from the compiler) and give power using adapter to docking station, the program never runs.....please help me what changes should I make in the code so that when I run the controller standalone and detach it from the compiler, It runs itself