This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CODECOMPOSER: Cannot set Skip Count on a breakpoint

Part Number: CODECOMPOSER

I'm running CCS 10.3.1.00003, communicating with an MSP EXP430FR5994 development board.

I have a single breakpoint set on a NOP instruction inside of a loop.

I'd like to set its skip count to 100, but it doesn't appear to take.  I've tried a bunch of things:

  • - Reload the code, halt at the entry point to main(), then try to set the skip count.
  • - Run the code up to the breakpoint then try to set the skip count.
  • - Run past the breakpoint at least once, then try to set the skip count

... but in every case, the skip count remains at 0.  When I say "set the skip count", my process is:

  1. Right click on the breakpoint in the breakpoint view, which brings up the context menu
  2. Select "Breakpoint Properties"
  3. Select the property for "Skip Count"
  4. Click on [Edit Property]
  5. Change the 0 to 100
  6. Click on [Apply And Save]

But the skip count remains at 0.

  • As I was typing this in, I stumbled upon the solution:

    After you click on [Edit Property] and enter the new skip count (steps 4 and 5 above), YOU MUST TYPE [ENTER] (or Return for the rest of us).

    Then the new Skip Count will take.